Module-defined Data Types (ETHERNET-PANELVIEW)
The table below lists and describes the Input and Output module-defined data types for this module, according to the Comm Format you've chosen.
Module-defined Data Type: AB:ETHERNET_PANELVIEW_INT_<n>Bytes:I:0
Comm. Format: Data - INT, Input Data - INT
Member Name | Data Type | Default Display Style |
Fault | DINT | Binary |
Data | INT[225] | Binary |
Module-defined Data Type: AB:ETHERNET_PANELVIEW_DINT_<n>Bytes:I:0
Comm. Format: Data - DINT, Input Data - DINT
Member Name | Data Type | Default Display Style |
Fault | DINT | Binary |
Data | DINT[112] | Binary |
Module-defined Data Type: AB:ETHERNET_PANELVIEW_INT_<n>Bytes:O:0
Comm. Format: Data - INT
Member Name | Data Type | Default Display Style |
Data | INT[225] | Binary |
Module-defined Data Type: AB:ETHERNET_PANELVIEW_DINT_<n>Bytes:O:0
Comm. Format: Data - DINT
Member Name | Data Type | Default Display Style |
Data | DINT[112] | Binary |
Provide Feedback