Failed to acknowledge alarm
Problem attempting to acknowledge the alarm. The error message indicates one of these conditions:
Acknowledge not required for this alarm
Cannot acknowledge an alarm that does not require acknowledgment. Check
Acknowledgment Required
in the Configuration dialog box to require the acknowledgment.This alarm has already been acknowledged
Cannot acknowledge an alarm that was already acknowledged.
Acknowledged with wrong parameters
Invalid parameters were sent with the acknowledge command.
Provide Feedback