Cam Editor Toolbar
![Camming toolbar](/content/dam/dita/en/studio-5000-logix-designer/37-00/help/rs5000/motion/cipmotion_gui_dialogs/camming/graphics/O2766.jpg/_jcr_content/renditions/cq5dam.web.1280.1280.jpeg)
This toolbar contains cam/cam profile editing functions.
TIP:
Tooltips on the toolbar indicate the intended use for each tool. Simply move your cursor over the icon and the tooltip appears. Note that Zoom In, Zoom Out, and Zoom-to-Fit are not available when you are using the Grid and Slope views.
Provide Feedback