Controller Organizer icons
The
Controller Organizer
window contains a hierarchy of the folders, files, and links that contain all of the information about the programs and data in the current project. The following table lists the icons that appear in the Controller Organizer
.Icon | Description | Icon | Description |
Open folder | Safety task | ||
Closed folder | Safety program | ||
Tags folder | Safety Add-On Instruction | ||
Continuous task | Sealed Add-On Instruction | ||
Periodic task | Sealed safety Add-On Instruction | ||
Program | Main safety ladder routine | ||
Alarms | Data type folder open | ||
Add-On Instruction | Data type folder closed | ||
Ladder routine | Data type | ||
Main ladder routine | Trend | ||
Function block routine | I/O Configuration fault open (shown online when any module is faulted) | ||
Sequential function chart routine | I/O Configuration fault closed (shown online when any module is faulted) | ||
Structured text routine | Backplane | ||
Equipment Phase | Module | ||
Equipment Sequence | Faulted module | ||
Locked routine | Safety module | ||
Locked Add-On Instruction | Ethernet | ||
Ladder phase state routine | NetLinx communications card | ||
Function block phase state routine | Coordinate system | ||
Sequential function chart phase state routine | Axis | ||
Structured text phase state routine | Link to the Logical Organizer |
For additional information about the
Controller Organizer
, see:Provide Feedback