Load a project from nonvolatile memory
Use the
Nonvolatile Memory Load/Store
dialog box to load a project from nonvolatile memory of the controller into RAM memory. Loading from nonvolatile memory overwrites the current controller image. Before you begin:
- Verify that the memory card is installed.
- Secure Digital cards have a lock feature. The card must be unlocked to write data to a Secure Digital card.ATTENTION:During a load, all active servo axes are turned off. Before you load a project, make sure that this will not cause any unexpected movement of an axis.
To load a project:
- Go online with the controller and put the controller inProgram Mode.
- On theController Propertiesdialog box, click theNonvolatile Memorytab, and then clickLoad/Store. TheLoad/Storebutton is unavailable when the:
- Nonvolatile memory is not present in the controller.
- Another user has locked the controller.
- Controller has redundancy enabled.
- Verify that the image in nonvolatile memory is the project you want to load.
- SelectLoad. TheLoaddialog box appears, prompting you to confirm the load.
- SelectYes.
- For safety applications, you are prompted to unlock the safety application if:
- The nonvolatile memory image and the controller are safety locked but the safety signatures do not match.
- The controller is safety locked.To start the load operation, selectUnlock. If the unlock is unsuccessful, theNonvolatile Memory Load/Storedialog box displays an error message.If the load is unsuccessful, an error message appears.
- Once the load is complete, selectOK.TIP:For safety applications, the controller's safety lock passwords and signature will always be set to the nonvolatile memory values after a successful memory load.
Provide Feedback