Equipment Phase Properties - Monitor Tab fields
Use the dialog to view run-time information of the
Monitor
tab of the Equipment Phase
PropertiesEquipment Phase
, including maximum and last scan times, the current sequence state, and its owner. These options are available on the Monitor
tab.
Item | Name | Purpose |
![]() | Max | Displays the maximum amount of scan time of the equipment sequence, in milliseconds. |
![]() | Last | Displays the last scan time of the equipment sequence, in milliseconds. |
![]() | Max Reset button | Resets the maximum and last scan times and restarts the scan timer. |
![]() | State | Shows the current state of the equipment sequence. Available states are: IDLE, COMPLETE, STOPPED, ABORTED, HELD, RESETTING, STOPPING, RUNNING, ABORTING, HOLDING, and RESTARTING. |
![]() | Substate | Shows the current substate for pausing of the Equipment Phase . Available substates are:
|
![]() | Owners | Shows the current owner(s) of the Equipment Phase . Available owners are:
|
OK | Select to accept edits. If all attributes are valid, the modified attributes save for the current Equipment Phase and this dialog closes. OK and Apply are unavailable if the dialog box contains invalid data. | |
Cancel | Select to cancel edits and close the Equipment Phase Properties | |
Apply | Select to apply edits and continue editing in the Equipment Phase PropertiesOK . |
Provide Feedback