Import/Paste Configuration dialog - Configure Connections tab settings
The table describes the settings and information displayed on the
Configure Connections
tab during an import.Setting | Description | ||||||||||||||||||||||||||||||
Parameter | Identifies an endpoint of the connection. The parameter identified in this box is the parameter in the import content that is to be connected to another parameter in the program that exists in the project. A New Connection option is available if the import content contains only one program. You can create connections that are not part of the import content by connecting a program parameter in the import content to an endpoint connection in a program that is in the project. The result is a new connection that did not previously exist in the import content nor in the program in the project. Type the parameter name for the new connection or click ![]() Parameters box, only the parameters that reside in the import content will be listed in the tag browser. When both the parameter and final connection have been specified, the connection is added to the connection grid after you move off the New Connection row or after you press Enter . If you enter an invalid parameter, the connection is not created and the error indicator appears in the leftmost column. Point to the error indicator to see a description for the cause of the error.The New Connection option is not available when you are importing:
| ||||||||||||||||||||||||||||||
Data Type | The data type of the parameter. A parameter can only be connected to a tag or a parameter with the same data type or an error occurs when you verify the program. | ||||||||||||||||||||||||||||||
Usage | Shows the usage type as Input , Output , InOut , or Public . | ||||||||||||||||||||||||||||||
Import Connection | Shows the name of the connection endpoint for the parameter from the import file. This box is blank if the connection is only defined in the program that exists in the project. | ||||||||||||||||||||||||||||||
![]() | Indicates if there are differences between the program that is in the import content and the program that is in the project. Also identifies if the program exists in the import content, or if it exists in the program that is in the project. Click the browse button in the Details column to see more extensive component properties.There are two at-a-glance indications of how the imported content matches the content of the program that exists in the project:
Point to the differences icon for a connection to see a tooltip that provides details about the connection. | ||||||||||||||||||||||||||||||
Operation | Identifies whether the connection will or will not be made upon import of the program into the project.
Operation box example.
Example
| ||||||||||||||||||||||||||||||
![]() | Select ![]() Connection Properties dialog, which lists parameter and connection properties. | ||||||||||||||||||||||||||||||
Final Connection | The parameter in the existing project that the import parameter will be connected to. If a connection in the Connection grid is only in the existing project, the value in the Final Connection box cannot be changed.You can change the value in the Final Connection box based on the value in the Operation box. You can type the final connection name or click ![]() If you enter an invalid final connection, the error indicator appears in the left column. Point to the error indicator to see a description for the cause of the error. Final Connection example.
Example
| ||||||||||||||||||||||||||||||
Messages | Messages about the import status appear below the grid. |
Provide Feedback