Align sequence elements in an Equipment Sequence diagram

Align the sequence elements in an
Equipment Sequence
diagram to minimize the
Equipment Sequence
diagram size and make the diagram appear with less visual clutter.
To align sequence elements in an
Equipment Sequence
diagram:
  1. Select two or more sequence elements.
  2. On the
    Menu bar, select
    Edit > Layout Selected Elements
    .
    TIP:
    Use keyboard short
    Ctrl + A
    or on the Menu bar, click
    Edit > Select All
    to select all sequence elements to align at one time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.