Function Block Properties dialog box - EU Scaling tab (CC)

The Coordinated Control (CC) instruction controls a single process variable (PV) by manipulating as many as three different control variables (CV). As an option, any of the three outputs can be used as an input to create feed forward action in the controller. The CC calculates the control variables (CV1, CV2, and CV3) in the auto mode based on the PV deviation from the set point (SP), internal models, and tuning.
Use the
EU Scaling
tab to set the Engineering Unit (EU) scaling values for the selected CC function block.
The following table describes the parameters available on the
EU Scaling
tab:
Parameter
Description
Process Variables
  • Max at 100% Span
Enter the maximum scaled value for PV, which is the value of PV and SP that corresponds to 100 percent span of the Process Variable.
Valid values are in the range of PVEUMin < PVEUMAX LessThanOrEqualTo maximum positive float.
The default value is 100.0
  • Min at 0% Span
Enter the minimum scaled value for PV, which is the value of PV and SP that corresponds to 0 percent span of the Process Variable.
Valid values are in the range of maximum negative float LessThanOrEqualTo PVEUMin
<
PVEUMax.
The default value is 0.0
Control Variables
  • Max at 100% Output
Enter the maximum value for CV1EU, CV2EU, and CV3EU. This is the value of CVEU1, CVEU2, and CVEU3 that corresponds to 100 percent CV1, CV2, and CV3 respectively.
The default value is 100.0
  • Min at 0% Output
Enter the minimum value for CV1EU, CV2EU, and CV3EU. This is the value of CVEU1, CVEU2, and CVEU3 that corresponds to 0 percent CV1, CV2, and CV3 respectively.
The default value is 0.0
Status
Displays read-only status information for blocks containing status bits. If none of the status bits are set, an OK message appears in this field. Otherwise, a list of the status bits that are set appears here. This list is comprised of the parameter names associated with the status bits, and typically explain which parameters were configured with invalid values.
Execution Order Number
Displays the block's execution number if the routine is in a verified state. If the routine is not yet verified, a
Routine not verified
message displays. Note that this item is read-only.
Never display description in a routine
Select this check box if you do not want the description to display in the routine.
OK
Click this button to add the selected item in the instruction list to the routine and close the Fun
ction Block Properties
dialog box.
Cancel
Click this button to cancel any edits you have made and close the
Function Block Properties
dialog box.
Apply
Click this button to accept your changes and continue editing in the
Function Block Properties
dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.