- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Go to a Grid Location
To go to a specific grid location in the Function Block or SFC editor
: - From theGo towhat list, selectGrid Location.
- In theMove to gridlocationbox, type the coordinates of the grid location to which you wish to go to (for example, B24).
- SelectGo To. The specified location is centered in the Editor window.
To access the Go To dialog box:
- To access theGo Todialog box, select the right mouse button while in the Ladder Editor and selectGo To. For more details, see Go To dialog box settings
Provide Feedback