About the Ladder Editor Caret

About the Ladder Editor Caret

The
Ladder Editor
provides a caret as an aid when editing ladder logic. This caret represents the current working position in the routine window. Additionally, each pane of each routine view contains its own caret, enabling work in two separate sections of a routine at one time.The caret only appears when the view is active.
When a routine first appears, the caret is located in the rung selection region of the first rung.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal