HMI navigation for PMTR
Use the
Navigation
tab on the PMTR Properties
dialog box to configure navigation from the HMI to additional devices or destinations for Process Motor (PMTR) instructions.To enable HMI navigation for PMTR instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theHMItab, selectNavigation.
- (Optional) To allow navigation to a device or destination from the HMI faceplate, selectAllow navigationfor each device.
- In theDevice objecttag name box, enter the controller path and the device tag. For example, the object tag name for an overload relay object could be /North_Area::[ProcessStrategies]M101_Ovld.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state, such asRunning,Stopped, orOut of service.
- Device issues. Displays fault conditions, such asFail to startorConfiguration error.
- SelectApply.
Provide Feedback