Change SFC Editor > Element Naming Preferences

Change SFC Editor > Element Naming Preferences

Use the
Workstation Options
dialog box to customize the behavior and appearance of the Logix Designer application. The
Categories
parameter contains a list of all options categories that can be configured. Element Naming preferences are used to automatically generate names for different language elements in the sequential function chart routine.
To change SFC Editor > Element Naming preferences:
  1. Select
    Tools > Options
    to open the
    Workstation Options
    dialog box.
  2. Select the
    SFC Editor >Element Naming
    category.
  3. Select the
    Create Tag with Language Element
    option to have the
    Logix Designer
    application automatically create a tag when inserting an element in the Sequential Function Chart Editor.
    • Generate Tag Name
      - choose this option for the application to create the tag name
    • Prompt for Tag Name
      - choose this option for the application to show a prompt to name the generated tag
  4. In the
    Base Name
    field, enter the prefix to use for each:
    • Step
    • Transition
    • Action
    • Stop
      Configure these prefixes to be any valid
      Logix Designer
      application tag name.
  5. Select
    Prefix with Routine Name
    ito include the name of the active routine with the prefix.
    If selecting this option, the routine name is added to the beginning of the tag name, followed by an underscore, followed by the prefix, another underscore, and the auto-generated 3-digit number (for example, MyRoutine_MyPrefix_001).
    TIP:
    The active routine name is added to the prefix for new routines created after the changes are made to the workstation options. Changes do not affect the current routine.
  6. Select
    OK
    to accept changes and close the
    Workstation Options
    dialog, or click any category to continue configuring the workstation options.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal