Change SFC Listing report preferences

Use the
Print Options
dialog to select the SFC information to include in the report.
To change SFC Listing report preferences:
  1. Open the Print Options dialog:
    • From the main menu, select
      File
      >
      Print Options
      .
    • From the
      Print
      dialog box, click
      Print Options
      .
  2. Select the
    SFC Listing
    category, and select or clear:
    • Shrink to Fit Page
      - set the magnification so the entire sequential function chart routine fits on one page.
    • Include Blank Sheets
      - print all sheets, including those which do not contain any logic.
    • Include SFC Element Properties Listing
      - include the Step, Transition, and Stop listings in the report; these items follow the SFC routine listing.
  3. Select
    OK
    to accept edits and close the Print Options dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.