Routine Properties dialog box - Auto-Naming tab overview (Sequential Function Chart routine)
This dialog box displays the names that are automatically be generated for different language elements in the selected sequential function chart routine. Edit the fields in this dialog to customize the prefixes used for this routine. Changing prefix information on this dialog does not affect tag names that were already generated. Changing prefix information does not affect the configuration choices made in the Workstation Options dialog. All newly-created routines use the configuration information specified in the Workstation Options dialog.
Parameter | Description |
---|---|
Step | Enter a prefix for the Step element name. |
Transition | Enter a prefix for the Transition element name. |
Action | Enter a prefix for the Action element name. |
Stop | Enter a prefix for the Stop element name. |
OK | Click to apply edits and close the Routine Properties dialog box. |
Cancel | Click to cancel edits and close the Routine Properties dialog box. |
Apply | Click to apply edits and continue editing in the Routine Properties dialog box. |
Help | Click for help on the General tab. |
Provide Feedback