SERCOSRingFault
Applies to: Servo Drive axes.
SERCOSRingFault is a Boolean attribute. It is set when a serious SERCOS communication fault has occurred. A SERCOSRingFault shuts down the module.
SERCOSRingFault is a recoverable condition. To clear a SERCOSRingFault reconfigure the 1756-M08SE motion module.
The occurrence of a SERCOSRingFault sets bit #4 of the ModuleFaults attribute, the ModuleFault attribute, and bit #1 of the AxisFault attribute.
Provide Feedback