Structured Text Element toolbar

The
Structured Text Element
toolbar is a tabbed toolbar which shows the instruction set as tabbed categories on the toolbar. When you click a category tab, the instruction toolbar just above changes to show that category of instructions.
TIP: In Logix Designer versions 37 and later, use the Instruction Toolbox to find and add instructions to structured text.
This toolbar also has two scrollbars: one for the tabbed instruction groups, and one for the instructions within a group. Simply click these scrollbars to move through the groups or instructions. You can also resize this toolbar by dragging on its left or right edges.
TIP:
Tooltips on the toolbar indicate the intended use for each tool. Simply move your cursor over the icon and the tooltip appears.
STEditor_ElementToolbar_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.