Delete a task
Each task contains the programs that it executes. To delete the task,first unschedule each program.
Safety tasks cannot be deleted.
To delete a task:
- Unschedule each program under the task.
- Select the task in theController Organizer.
- From theEditmenu, chooseDelete.
- When the confirmation dialog appears, clickYesto delete the task.The task no longer appears in theController Organizer.
Provide Feedback