Change trend preferences

Change trend preferences

To change trend preferences:
  1. Select the
    Trends
    category.
  2. In
    Default Sample Period
    , enter the value you want to use as the sample period for most trends.
    When you create a new trend or a quick trend, this value is automatically used as the sample period, unless you specify another value. Valid values are in the range from 1 millisecond to 30 minutes; the default value is 10 milliseconds
  3. Under the
    Logging
    heading, choose the
    Trend Log Directory
    .
    In
    Trend Log Directory
    , enter the directory where you want to save permanent trend log files.
    Trend log files are generated when the trend is turned on. You can save them by specifying a directory for them. By default, they are saved in the project directory.
  4. Select
    OK
    to close the
    Workstation Options
    dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal