Date:
Original Event Date:
April 17, 2024
Time: 10:00 A.M. - 11:00 A.M. Central European Summer Time
Duration: 60 Minutes
Language: English
Webinar Help?
EMEAWebinars@ra.rockwell.com
If you're exporting panels and machines to North America, then it's vital that you're aware of the requirements of the UL508 standard. In particular, it sets out the key facts on how starter types in branch motor circuits should be selected.
Join this special webinar to find out:
- The most up-to-date information on UL508 and what it means
- Why understanding the regulation is so important
- How this should influence your starter type selection process