Change device properties
Configure properties for a device in the
Device list
tab. You can create or delete a device and view the tags of the device. You can open both Properties
for a device and view the profile of a device from Device list
. - On the explorer bar, selectDevices.
- InDevicesexplorer, selectDevice list.
- In theDevice listrow for the device, double-click the cell to change:
- Name. Change the name of the device.
- Description. Change the description of the device.
- Revision. Change the minor portion of the Revision after the decimal point.
- Press the Enter key or select another cell or item inDevice list. The new device properties are saved automatically.TIP: To view the profile of a device, inDevice list, right-click the device and selectOpen device properties. TheOverviewview opens.
Provide Feedback