Unassign a device

Unassign a device to remove its association with a parent device. When you unassign a device, all its connections are removed from the project and the device moves to the Unassigned folder as an existing device.
TIP: To reassign a device, see Add an existing device.
Unassign devices from the
Devices
explorer.
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. In
    Devices
    explorer, right-click the device and select
    Unassign
    .
    Select
    Unassign
    in the confirmation dialog. The device moves to the
    Unassigned
    folder.
NOTE: When you unassign a device, the devices assigned to it become unassigned, and on rack optimized devices, the device connection type reverts to the default setting, Data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.