EPMS wiring and programming example
This topic demonstrates how to wire the Guard I/O module and the instruction in the safety control portion of an application.
TIP:
The standard control portion of the application is not shown in the following diagram.
Wiring Diagram
Programming Diagram
This programming diagram shows the instruction with inputs and outputs.
Ladder Diagram
Module Definition
The following sections provide examples of how to use the programming software to set the
Guard I/O
module configuration operandsRockwell Automation suggests selecting
Exact Match
for the Electronic Keying
as shown. Compatible
Match
is also acceptable.Module Input Configuration
Module Output Configuration
Provide Feedback