Execution
Math status flags are set for the CV output.
Condition | Function Block Action | Structured Text Action |
---|---|---|
Prescan | InstructionFirstScan is set | InstructionFirstScan is set |
Instruction First Scan | If CVFault and CVEUSpanInv are set, see Processing Faults. If CVFault and CVEUSpanInv are cleared:
| |
Instruction first run | ProgOper is cleared.
The instruction changes to manual mode. | ProgOper is cleared.
The instruction changes to manual mode. |
EnableIn is cleared | EnableOut is cleared, the instruction does nothing, and the outputs are not updated. | N/A |
EnableIn is set | The instruction executes.
EnableOut is set. | EnableIn is always set.
The instruction executes. |
Postscan | No action taken. | No action taken. |
Provide Feedback