Configure a non-isolated analog output module- floating point
Create a channel-level configuration specific to your application.
To configure a non-isolated analog output module (floating point):
- Enter the appropriate
- In theController Organizer, right-click the module and selectProperties.
- In theModule Properties dialog, select theConfigurationtab.
- Select theChannelbutton to select the channel to configure.
Scalingvalues for:- Low Signal
- Low Engineering
- High Signal
- High Engineering
- In theOutput Rangebox, select the output range of the module.
- In theSensor Offsetbox, enter a value to compensate for sensor inaccuracies during calibration.
- SelectHold for Initializationto have the module hold the output signal unchanged until the output value (received from the controller) is within 0.1% of full scale of the value held.
- SelectApplyto save the changes and continue editing, or selectOKto save the changes and close the dialog.
Provide Feedback