Diagnostic Latching

This latching feature affects most of the diagnostic features, but there are a few it does not affect. The table specifies which features are affected and which are not.
Input/Output:
Affects:
Does Not Affect:
input
  • Open Wire Diagnostic
  • Loss of Field Power Diagnostic
output
  • No Load Diagnostic
  • Output Verify Diagnostic
  • Field Power Diagnostic
  • Short Circuit/Overload Diagnostic
  • Pulse Test
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.