Danger: Scheduling programs online affect safety task
You are attempting to schedule a program or programs while the system is online by dragging
them to a Safety task in the
Controller Organizer
. Scheduling
programs while online changes the execution of programs and may have unintended
consequences.Select
OK
to schedule the program(s), or select Cancel
to not schedule the program(s).Note that you cannot do the following when online or offline:
- Drag a standard program to a Safety task in theController Organizer.
- Drag a safety program to a standard task in theController Organizer.
Provide Feedback