Failed to create trend
There was a problem creating or modifying the trend. The error message indicates one of the following conditions:
The name is invalid
You entered an invalid name or a name that does not follow the IEC1131 naming standard. Reenter the name using the format defined by the standard.
Trend already exists
You tried to name or rename a trend to a name that is already in use by another trend. Choose a different name for this trend, or rename the existing trend.
Access denied
You do not have Security privileges to create a trend. Check with your Security Administrator to be sure you have sufficient access to the project.
Provide Feedback