Industrial applications such as real time analytics or data gateways are often best deployed at the edge, close to the plant assets, when high speed execution is required. However, deploying and managing multiple applications at the edge across your plant or fleet of plants can come with challenges such as high maintenance costs, a lack of flexibility and a lax security posture. Join us for this webinar to learn about these challenges of the industrial edge and how FactoryTalk Edge Manager helps address them.
We'll discuss how FactoryTalk Edge Manager provides a complete solution including industrial edge PCs on which the apps are deployed and a cloud instance that allows the user to perform centralized and more secure device, fleet and app management. Finally, we'll share a customer success story that highlights how FactoryTalk Edge Manager is being used today to help reduce risk, time and resources required for edge app deployment, management and orchestration.