Allen-Bradley FLEX I/O Dual-port EtherNet/IP communication adapters simplify network design and increase network resiliency
MILWAUKEE, July 2, 2012 — Machine and equipment manufacturers (OEMs), system integrators and end users with demanding applications look to simplify network design while maintaining resiliency. The new Allen-Bradley FLEX I/O dual-port EtherNet/IP adapters from Rockwell Automation achieve this goal – helping OEMs connect machines to their end customers’ IT infrastructures using a single network. With the dual ports, users can also leverage the adapter to display diagnostics via a simple Web browser, helping reduce troubleshooting and downtime.
The new EtherNet/IP adapters support a device-level ring (DLR) topology, which provides robust network infrastructure and extremely fast recovery time, while keeping implementation cost down. DLR infrastructures are connected at the end device versus the switch. With no need for unnecessary switches and cabling, users can reduce design time and simplify implementation. The ring also adds a measure of redundancy that is very effective when a connection fails – as a single network failure, such as a cable break, will not lead to the failure of the other devices in the ring. A DLR network can recover in less than 3 milliseconds for a 50-node system. During this time, the connection between the programmable automation controller and the I/O device is not interrupted. The adapters also support the daisy-chain topology for applications that involve devices located long distances from CPU subsystems.
The adapters (1794-AENTR and 1794-AENTRXT for extreme environments) are compatible with these Rockwell Software products: RSLogix 5000 programming software version 16 and higher and RSLinx version 2.58 and higher. The adapters also can connect up to eight FLEX I/O modules.
About Rockwell Automation
Rockwell Automation, Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs over 21,000 people serving customers in more than 80 countries.
For more information:
- 1794 FLEX I/O Dual-Port EtherNet/IP Communication Adapter Module:
http://ab.rockwellautomation.com/IO/1794-FLEX-IO-Communication-Interfaces - 1794 FLEX I/O Dual-Port EtherNet/IP Communication Adapter Module photo:
http://www.flickr.com/photos/rockwellautomation/7454970400/in/photostream
Media contacts:
Gigi O’Neill
Rockwell Automation
404.646.3192
ggoneill@ra.rockwell.com
Sarah Kalhorn
Padilla Speer Beardsley Inc.
612.455.1791
skalhorn@padillaspeer.com
Allen-Bradley, FLEX, LISTEN. THINK. SOLVE., Rockwell Software, RSLinx and RSLogix are trademarks of Rockwell Automation, Inc.EtherNet/IP is a trademark of ODVA.
Published July 1, 2012