Supported Fields for the Events Table

Supported Fields for the Events Table

The following table provides the supported fields for the Events table:
Supported Fields for the Events Table
Column Name
Column Type
Description
Example
id
bigint
A server-generated ID for the object.
454501654069443
createdTime
timestamp
Timestamp when event was created.
2019-09-07T15:50+00Z
lastUpdatedTime
timestamp
Timestamp when event was updated.
2019-09-07T15:50+00Z
externalId
varchar
The external ID provided by the client. It must be unique for the resource type.
CDF_ExternalID
dataSetId
bigint
The ID of the dataset this asset belongs to.
7166729101688251
type
varchar
Type of the event. For example: 'failure'.
failure
subtype
varchar
Sub-type of the event. For example: 'electrical'.
electrical
description
varchar
Textual description of the event.
CDF project: testing_purpose
source
varchar
The source of the event.
FTDM
endtime
timestamp
Timestamp
2019-09-07T15:50+00Z
startTime
timestamp
Timestamp
2019-09-07T15:50+00Z
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.