- Extractors
- Analyze Data
Supported Fields for the Timeseries Table
The following table provides the supported fields for the Timeseries table:
Column Name | Column Type | Description | Example |
---|---|---|---|
id | bigint | A server-generated ID for the object. | 454501654069443 |
createdTime | timestamp | Timestamp when timeseries data was created. | 2019-09-07T15:50+00Z |
lastUpdatedTime | timestamp | Timestamp when timeseries data was updated. | 2019-09-07T15:50+00Z |
isString | bool | True if the time series contains string values; false if it contains numeric values. | true |
isStep | bool | It defines whether the time series is a step series or not. | true |
externalId | varchar | The externally supplied ID for the time series. | CDF_ExternalID |
name | varchar | The display short name of the time series. | function-variable-test |
unit | varchar(32) | The physical unit of the time series (free-text field). | Meter/sec |
assetId | bigint | The asset ID of equipment linked to this time series. | 1027806836454786 |
description | varchar | Description of the time series. | CDF project: testing_purpose |
dataSetId | bigint | The dataSet Id for the item. | 7166729101688251 |
Provide Feedback