Supported Versions

Supported Versions

The following Tableau versions are supported by virtual Postgres interface:
  • For Tableau Server, the supported version is 2024.2.2.
  • For Tableau Desktop, the supported version is 2024.2.2.
  • For Tableau Cloud, the supported version is 2024.2.0.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.