Automatic data refresh of reports in Power BI Service

Automatic data refresh of reports in Power BI Service

Prerequisite:
  • Power BI Gateway is installed, up and running.
Follow the instructions to publish report to a workspace on Power BI Service and perform the data refresh:
  1. In the Power BI Desktop application, navigate to
    Home
    >
    Publish
    .
    The
    Publish to Power BI
    dialog box is displayed.
  2. Select the workspace from the list of workspaces.
  3. Click
    Select
    to publish.
    When publishing is complete, a
    Publishing to Power BI
    dialog box is displayed which allows you to navigate to your report on Power BI Service.
    Publish PowerBI
    Now your Power BI Service is ready to use with DataMosaix and Power BI Gateway. To learn more about data refresh, refer to Data refresh in Power BI.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.