Register an FT Historian (OSI PI) Extractor

Register an FT Historian (OSI PI) Extractor

Perform the following steps to register an FT Historian (OSI PI) extractor:
  1. On the Management Console, select the
    Extractor Info
    tab.
    The Extractor list is displayed.
    Extractor Info tab
  2. Click the Add [+] icon.
    The
    Extractor Info Detail
    page is displayed.
    Extractor Info Detail Page
  3. Provide a unique name for your Extractor. The Source Name works as the identifier for your extractor. You can search for an extractor with the Source Name. By default, DataMosaix generates a source name.
    Source Name example: EXT_1406230728_createproject_v1.
    Here, EXT stands for extractor, 140623 is the date in ddmmyy format, 0728 is the timestamp in hhmm format, and createproject_v1 is the project in which you are currently working. You can use the default source name or create your own.
  4. Provide the location details for which you are creating the extractor. This information can help you to identify an extractor when you have many extractors for different plants/sites/locations.
  5. From the Associated Roles drop-down list, select at least one role. You can refer to various roles and capabilities by clicking
    Role Reference
    .
    You can select multiple roles from the Associated Roles drop-down list. In the search bar, you can search for any specific role from the list. If you want to apply all the roles to the application, select the
    Select All
    checkbox.
    NOTE:
    The Associated Roles drop-down is visible and available only for Project Admin users or users within the Organization with a Project Admin Role assigned.
    Next, you can select a pipeline or create a new pipeline. When you create a new pipeline, you have the option of selecting from an existing dataset or creating a new dataset.
  6. From the pipeline drop-down, select a pipeline. On selecting a pipeline, the Pipeline External ID and Dataset Name fields are populated.
    To create a new pipeline, select the
    + Create Pipeline
    option.
    The Create Pipeline dialog box is displayed.
  7. Provide the following Pipeline information to create a new pipeline:
    • Pipeline Name
    • Pipeline External ID
    • Pipeline Description
  8. When you create a pipeline, you can either select an existing dataset or create a new dataset. Select a Dataset from the drop-down if you want to use an existing Dataset.
    If you choose to create a new Dataset, the Dataset related fields are displayed. Provide the following dataset information:
    • Dataset Name
    • Dataset Description
  9. Click
    Add
    . Based on the options you choose (select or create), the Pipeline and Dataset information is either generated or created and displayed on the Extractor Info Detail page.
  10. Select the source type of extractor as
    FT HISTORIAN (OSI PI)
    .
    The fields relevant to the FT Historian (OSI PI) extractor appear on the screen for you to fill in details.
    Extractor Info Detail - FT Historian (OSI PI) Extractor
  11. In the PI Host, provide the hostname or IP address of the OSI PI server that you want to connect to.
    You can leave the OSI PI server username and password fields empty.
  12. In the Username and Password fields provide the credentials to connect to the PI Host if you need it. If the PI host server is on local host you can leave it blank.
    NOTE:
    The Save and Apply button enables only after you provide all the required details.
  13. Click
    Save and Apply
    .
    The
    Generated info Saved
    dialog box is displayed and it contains the configuration information. You can view the configuration file details by clicking
    View generated configuration file
    . Alternatively, you can also copy and save the information for future use by clicking
    Copy All
    . You can also download the config.yml file that includes all the configuration information that you can use to run the extractor.
    Extractor Configuration File Download
  14. Click
    Download
    .
    The config.yml file is downloaded in the Downloads folder of your local machine.
  15. Click
    Close
    to close the dialog box.
    The new extractor is displayed under Extractor Listing.
  16. Navigate to your project in CDF by clicking [Continue to Main Site] and select
    Integrate
    >
    Connect to source systems
    .
    Connect to Source Systems
  17. On the Extract data screen, locate the
    Rockwell FactoryTalk Historian SE
    extractor and select it.
    Cognite PI Extractor
  18. Download the PI extractor msi file from CDF.
  19. Copy the downloaded config.yml file to the folder where the extractor is installed. The default location is: C:\Cognite\PiExtractor\config. You must paste the copied config.yml file into the 'config' folder.
  20. Run the extractor on the command line.
    Alternatively, you can run the PI extractor as a Windows service. To learn more, refer to Run as a Windows service.
  21. Once the extractor has been configured and executed successfully, navigate to your project in CDF Project and open the pipeline by selecting
    Integrate
    >
    Monitor Extractors
    .
  22. Click the pipeline link.
    You should see the information mentioning that the extractor has run successfully.
    Extractor Success Info
  23. Click on the Data set link under basic information section to open the Data set details.
    Data Set Details
  24. Click on the Data tab.
    You should see the asset and time series data. You may also see Assets depending on the configuration of the namespace on the PI Server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.