Configuring FT Optix to connect to DataMosaix

Configuring FT Optix to connect to DataMosaix

Make sure that you have installed the FactoryTalk Optix Studio application on your system. Once you select the source type as FT Optix in the Source Info section, a link to download the application will appear (Get FactoryTalk Optix). You can also download the FactoryTalk Optix Studio from FactoryTalk Hub. For more information on installation, refer to Install FactoryTalk Optix Studio.
Perform the following steps to configure FT Optix to connect to DataMosaix:
  1. Launch the FactoryTalk Optix Studio application.
  2. To open a FT Optix project:
    • For existing projects, click any project from the
      Recent projects
      section.
      Open Existing Project
    • For a new project, click
      New
      [+].
  3. Provide the
    Name
    and
    Location
    details.
    New FT Optix Project
  4. Click
    Create
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.