Prerequisites
- A project is created using FactoryTalk DataMosaix.
- FactoryTalk Optix Studio and FactoryTalk Optix DataMosaix Connector (FT DataMosaix_Optix_Connector.msi file) are installed on your system.
NOTE:
Make sure that the
FTDM-FTOptix FTDataMosaix Connector
feature is enabled in the Manage Access > Features tab. For more information, refer to Enable or Disable Features.Provide Feedback