Supported Extractor Versions

Supported Extractor Versions

The following extractors are supported by the configuration UI. Other extractors are supported using the Customer/Other extractor type:
  • ODBC Extractor
    : v 3.0.0
  • OPC UA Extractor
    : v 2.18
  • OSI PI Extractor
    : v 4.1.0
  • FT Optix Connector
    : v 1.02.00
  • Asset Framework (PI-AF) Connector
    : v 1.5.1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.