Deactivate Features

Deactivate Features

Perform the following steps to deactivate features:
  1. On the Management Console, navigate to
    Manage Access
    >
    Features
    .
    The Features page displays the available features with a short description and the date they were last updated in the feature management platform.
  2. Turn the toggle button to
    Inactive
    .
    The Confirm Deactivation dialog box is displayed.
    NOTE:
    When you deactivate a feature, it becomes unavailable to all users of the selected project.
  3. Click
    Deactivate
    .
    Deactivate Feature
    You will be notified that the selected feature has been successfully deactivated.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.