- Extractors
- Analyze Data
Navigation
The home page of FactoryTalk DataMosaix features a left navigation menu with the following tabs:
- Manage Access
- Extractor Info
- Applications
- Modeling
On the left navigation menu, you can also find direct links to Main DataMosaix (Cognite Data Fusion) and FactoryTalk Hub.
Left Navigation Menu

Manage Access | Allows you to modify users' roles using the Members sub-tab. You can view, edit, and modify the default and custom Capability Groups and Roles associated with the organization. Also, you can activate or deactivate a specific functionality in DataMosaix using the Features sub-tab. |
Extractor Info | Allows you to register extractors that helps to push data to FactoryTalk DataMosaix. |
Applications | Allows you to register applications that helps to view data. |
Modeling | Allows you to create assets and helps organize assets and their properties in a hierarchical structure. |
Provide Feedback