- Extractors
- Analyze Data
Remove Role
If you are a project administrator, you can remove any assigned roles or all of them.
Perform the following steps to remove the roles:
- On the Management Console, select theManage Accesstab.
- In theActionscolumn, click the [
] icon of the desired users.
Member ListingNOTE:If any or all roles are assigned to the member, the [] icon is enabled. If no roles are assigned to the member, the [
] icon is disabled.
TheRemove Rolespage displays the assigned roles.NOTE:Click the [] icon to expand the role and view its capabilities. Click the icon again to collapse it.
Role Capabilities - Select the checkbox adjacent to a role.NOTE: The user can use the search bar to find a specific role.You can select multiple roles by selecting the required checkboxes. To remove all the assigned roles, select theRolesheader checkbox.
- ClickRemove.The "Roles updated" message is displayed.Remove Roles
Provide Feedback