Remove Roles from Multiple Members

Remove Roles from Multiple Members

If you are a project administrator, you can remove assigned roles from multiple members using this feature.
Perform the following steps to remove roles from multiple members:
  1. On the Management Console, select the
    Manage Access
    tab.
  2. To remove roles from multiple members, select the checkboxes adjacent to the members' names.
    The [+] and [] icons above the member grid are enabled or disabled based on the roles assigned to the selected members.
    • If no roles are assigned to any of the selected members, the [+] icon is enabled and [] icon is disabled.
    • If all the roles are assigned to all the selected members, the [+] icon is disabled and [] icon is enabled.
    • If some roles are assigned to any of the selected members, then both, the [+] and [] icons are enabled.
  3. Click the [] icon above the
    Member Name
    column.
    Bulk Remove Roles from Members
    The
    Remove Roles
    page displays the list of available roles with a number next to each role name. The number in the parentheses denotes how many members out of the selected members are currently assigned to a role. The user can click the number in the parenthesis to view the assigned member details.
    Members Assigned to a Role
  4. Select the checkboxes adjacent to the roles you want to remove. Selecting the checkboxes will remove those roles from the members that are currently assigned the role
    NOTE: The user can use the search bar to find a specific role.
    You can remove all the assigned roles, by selecting the
    Roles
    header checkbox.
  5. Click
    Remove
    .
    The "
    Roles updated
    " message is displayed.
    Bulk Remove Roles
    NOTE:
    Click the [] icon to expand the role and view its capabilities. Click the icon again to collapse it.
    Role Capabilities
NOTE:
For more information on CDF Access Management, refer to this link.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.