Device definition
Use these elements to define a device. These elements are common to all device definitions.
deviceCategory
defines the type of device.Element | Description |
---|---|
ControllerDevice | Defines this instance as a controller. |
CipDevice | Defines this instance as an active device, such as an adapter, an IO device, and so on. |
Provide Feedback