Develop an interface for switching locales
Create a localized label and two buttons that change the interface language.
Application example - English locale
![](/content/dam/dita/en/factorytalk-optix/current/_images/SwitchingLocales1.png/_jcr_content/renditions/original)
Application example - Polish locale
![](/content/dam/dita/en/factorytalk-optix/current/_images/SwitchingLocales2.png/_jcr_content/renditions/original)
NOTE:
Download a sample project:
SwitchLocales.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example
![](/content/dam/dita/en/factorytalk-optix/current/_images/SwitchingLocalesDesign.png/_jcr_content/renditions/original)
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback