Basic entitlement on ASEM 6300 iPC
entitlement
on ASEM 6300 iPC
The Access Server assigns a Basic entitlement to Windows FTRA Runtimes on these devices.
To upgrade a Basic entitlement for any FactoryTalk Remote Access Runtime installed on any ASEM hardware:
- Access FactorytalkHub.com and clickUpgradenext to the Basic entitlement that you own.
- Choose a Pro entitlement from the available entitlements list.
NOTE:
The Pro entitlement deactivation restores the Runtime Basic entitlement.
NOTE:
Basic entitlements are set as per factory settings.
Provide Feedback