Getting Started
FactoryTalk® Remote Access™ is the Rockwell Automation software solution that enables remote access and remote assistance to industrial equipment associated with Ethernet and serial connections through the Stratix® 4300 Remote Access™ Router, or through industrial PCs with the FactoryTalk® Remote Access™ Runtime installed.
Before you begin, review information about FactoryTalk Remote Access subscriptions, how resources are organized into remote access domains, how to perform the initial configuration of Stratix® 4300 Remote Access™ Routers, how to download and install the FactoryTalk Remote Access Runtime, how to download and install FactoryTalk Remote Access tools, and the initial configuration to set up your organization with FactoryTalk Remote Access.
Provide Feedback