Runtime connection and registration (do not use)

A device can be connected to a network and to a domain, whereas its
entitlement
needs to be
registered
. To activate Runtime,
an entitlement
registration is mandatory.
NOTE: You can register a device to a domain while the same device is registered to another domain, if the domain it is registered to has an expired Trial entitlement.

Ubuntu 22 device connection

  1. When the Runtime is running, connect to the
    FactoryTalk Remote Access
    network infrastructure by entering the following commands:
    cd /opt/Rockwell_Automation/FactoryTalk_Remote_Access/Runtime/bin FactoryTalkRemoteAccessRuntimeCli --connect
  2. If the Runtime needs to join an organization/domain, once the Runtime is connected to the
    FactoryTalk Remote Access
    network infrastructure run the command:
    FactoryTalkRemoteAccessRuntimeCli --getAnonymousID
  3. The ID and the password used to join the organization/domain will display.
  4. Access
    FactoryTalk Remote Access Manager
    and the
    Explorer
    Domain view
    section and open the folder where you wish to store the remote device and click on the
    Add resource
    (
    circled plus
    ) button, then select
    Add device
    .
  5. Select
    Add device remotely
    and enter the remote device ID and password obtained when selecting
    Connection
    on the Linux/Ubuntu Device Manager.
NOTE: You can check whether a device is registered both through the
FactoryTalk Remote Access Manager
on the right pane of the
Explorer
Domain view
section, or on the Windows Runtime, on the
Information
(
circled 'i'
icon) section.

Hardware identification

Upon its first connection to the network, Runtime stores its identity on the device disk in a file named
auth.bin
. The location of this file depends on the system used, as indicated in the following table.
Runtime for third party devices
System
Path
Windows 10
C:\ProgramData\Rockwell Automation\FactoryTalk Remote Access\Identity
Linux Ubuntu 22
/opt/FactoryTalk_Remote_Access/Identity/
Runtime for Rockwell Automation devices
System
Path
Stratix 4300 Routers, OptixPanels graphic terminals, Embedded Edge Compute Module
/persistent/data/Rockwell_Automation/FactoryTalk_Remote_Access/Identity/
NOTE: It is not possible to transfer the identity file from one device to another by copying the
auth.bin
file. However, you can create a backup of the file and restore it after uninstalling and reinstalling the operating system or Runtime.
The only scenario in which you cannot restore the identity file is when the disk is replaced. In this case, the device is recognized as a different machine.

Keep-alive feature

The data exchanged for the keep-alive feature between Runtime and the server infrastructure and between
FactoryTalk Remote Access Manager
and the server infrastructure is approximately 1 KB per minute.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.