FactoryTalk Remote Access entitlement activation
- To purchase entitlements, go to the Rockwell Commerce page https://commerce.rockwellautomation.com/ and log in with your MyRockwellAutomation account.
- EnterFactoryTalk Remote Accessin the webpage search bar and select the entitlement that you wish to purchase. Then, click on the shopping cart to proceed with your purchase.
- Access FactorytalkHub.com and click on the
icon.
- SelectView entitlements: here you can purchase or allocate entitlements.
- Once you have purchased an entitlement, it appears in theAvailable for allocationlist.
- Click theAllocatebutton next to the purchased entitlement and confirm.NOTE: The entitlement is not yet associated to the service.
- Access FactoryTalk Remote Access Manager and selectDomain view.
- Select the device for which you wish to activate an entitlement and click on the circled plus icon next to theEntitlementpane on the right.
- Select the purchased entitlement from the displayed list and associate it to your device.
If a device hosing Runtime becomes inoperable, it is possible to temporarily move the entitlement to another device, while the first one is being repaired. To do so:
- Access FactoryTalk Remote Access Manager and theDomain viewsection.
- Select the inoperable device and access the relatedEntitlementspane.
- Disassociate the entitlement. The entitlement will be moved to theAvailable for allocationlist.
- Associate the entitlement to a temporarily replacing device as per procedure.
- Disassociate the entitlement from the temporarily replacing device and associate it back to the repaired device.
NOTE:
You can check whether a device is registered both through the FactoryTalk Remote Access Manager on the right pane of the
section, or on the Windows Runtime, on the Information
(circled 'i'
icon) section.Provide Feedback