OptixPanel™ graphic terminals
™
graphic terminalsOptixPanel
™
Graphic Terminals integrate both FactoryTalk Optix and FactoryTalk Remote Access Runtime. Terminals are available in two configurations:- OptixPanel: It is provided with a Pro Runtime entitlement.™Standard Graphic Terminal
- OptixPanel: It is provided with a Basic Runtime entitlement and allows to purchase an entitlement upgrade.™Compact Graphic Terminal
NOTE:
See Entitlements for more information about this subject.
NOTE:
For further information on the OptixPanel
™
Graphic Terminals, see the documentation provided at the link https://www.rockwellautomation.com/en-us/products/hardware/allen-bradley/new/optixpanel-graphic-terminals.htmlThe image below shows the the
FT Optix
section in System Manager.Provide Feedback