(Interactive Access) Explorer

This section allows you to transfer files between local and remote devices. In
Explorer
you can carry out remote file operations, such as download, upload, rename, and delete files. You can click the
play symbol
next to an executable file installed in the remote device to start it.
You can monitor file transferring processes through a practical two-panes view, showing both the root and the receiving folder paths.
This section is split in two panes: the left panel displays the files the local device running the
FactoryTalk Remote Access Manager
, while the right pane shows the files the remote device.
To access the
File Transfer
pane, proceed as follows:
  1. Make sure that the
    FactoryTalk Remote Access Manager
    is connected to the remote device.
  2. Access the
    Explorer
    Device view
    section.
  3. Click the
    Interactive Access
    Tool button, then select
    Explorer
    .
    NOTE: See Interactive Access for further information on this Tool.
NOTE: File Transfer operates with local system privileges. This means that the
FactoryTalk Remote Access Manager
admin can enable or disable specific operations for remote users.
Once you have selected the files that you want to transfer, click
Send
or
Receive
, as needed.
NOTE: In case the file transfer is interrupted for any reason, it can be resumed or restarted by clicking
Resume
or
Resume all
.
To rename a file or folder, right-click it and select
Rename
in the context menu.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.